Version notes for SWD-Assist
Date: 7-Sep-2021


Version notes for SWD-Assist V3.00
Version notes for SWD-Assist V2.80
Version notes for SWD-Assist V2.75
Version notes for SWD-Assist V2.70
Version notes for SWD-Assist V2.62
Version notes for SWD-Assist V2.61
Version notes for SWD-Assist V2.60
Version notes for SWD-Assist V2.50
Version notes for SWD-Assist V2.40
Version notes for SWD-Assist V2.30
Version notes for SWD-Assist V2.20
Version notes for SWD-Assist V2.10
Version notes for SWD-Assist V1.92
Version notes for SWD-Assist V1.90
Version notes for SWD-Assist V1.80
Version notes for SWD-Assist V1.71
Version notes for SWD-Assist V1.70
Version notes for SWD-Assist V1.60
Version notes for SWD-Assist V1.50
Version notes for SWD-Assist V1.41
Version notes for SWD-Assist V1.40
Version notes for SWD-Assist V1.30
Version notes for SWD-Assist V1.20
Version notes for SWD-Assist V1.10
Version notes for SWD-Assist V1.01
Version notes for SWD-Assist V1.00


Version notes for SWD-Assist V3.00:

Modifications in V3.00:

In SWD-Assist contained SWD device catalog version: V1.10

SWD device catalog:

The SWD device catalog has been changed in order to be able to install catalog updates as separate updates. The current version of the SWD device catalog is displayed together with the version of SWD-Assist in the info dialog.

In the device catalog are now tooltips displayed showing device name, order numbers and supported profiles of cyclic data if the module supports multiple profiles.

Support for high display resolution settings:

The SWD-Assist supports now high display resolution settings. The resolution of the primary monitor is used. (when multiple monitors are used)

Update check:

The update check has been integrated into the SWD-Assist. The updates for the SWD-Assist and for the SWD device catalog are displayed in a window of the SWD-Assist. The installation of an update can be started directly out of that window. Alternatively the update files can be downloaded and installed manually.

EU5C-SWD-EIP-MODTCP gateway: Tag list export

When the EU5C-SWD-EIP-MODTCP Gateway is used in EIP mode, an simplified tag list without single bit definitions can be exported. In the simplified tag list multiple single bits in one byte are exported as one byte entry. The export of the simplified tag list can be triggered via a separate menu entry.

The following device has been added to the device catalog:

Change of protection type of M12 modules:

In the description text of the M12 I/O modules the protection type has been changed from IP67 to IP69K.

Changes regarding Hytrol:

Note on the "Save GSD file..." function in connection with the PXR-RCAM-SWD device:

If the "PXR-RCAM-SWD" device is present in the SWD configuration, it will not be possible to use the import of an exported GSD file in TIA Portal and STEP7.
Unintentional termination of the application may occur here.
In this case, the configuration should be done manually in the respective software using the general GSD files for the EU5C-SWD-DP device.

Back


Version notes for SWD-Assist V2.80:

Modifications in V2.80:

Changes for the gateway EU5C-SWD-PROFINET:

This gateway supports now up to 2 MBaud for SWD communication. (At least firmware version 1.5.0.0 is required)

Changed device name:

The device name "DXG-NET-SWD-IP21" in SWD-Assist has been changed to "DXG-NET-SWD-IP20".

Back


Version notes for SWD-Assist V2.75:

Modifications in V2.75:

The following devices have been added to the device catalog:

New Parameter added to M22-SWD-INC:

By this parameter the diagnostic message can be disabled when the button is pressed too long. This parameter is supported from Firmware-Version VX.XX and up in the device M22-SWD-INC. Prior firmware versions ignore this new parameter.

Back


Version notes for SWD-Assist V2.70:

Modifications in V2.70:

The following XV303 variants have been added to the device catalog:

The following network components have been added to the device catalog:

The following devices have been added to the device catalog:

Back


Version notes for SWD-Assist V2.62:

Modifications in V2.62:

The following devices have been added to the device catalog:

Notes on the device catalog and "Phoenix Contact" device catalog mode:

The following Phoenix-Contact devices have been removed from the catalogue.:

The "Phoenix Contact" catalog mode is removed from SWD-Assist. Old projects can be opened and modified. If possible, the devices are replaced by EATON devices.

Bug fixes:

Errors in the current/voltage calculation for supply voltages >24V have been corrected.

Back


Version notes for SWD-Assist V2.61:

Modifications in V2.61:

Support for dimmable RMQs:

Dimmable RMQs are now supported. The brightness level is displayed as an additional output for all RMQs with LEDs. No distinction is made between non-dimmable RMQs and dimmable RMQs. RMQs without dimming function ignore the brightness setting.

Back


Version notes for SWD-Assist V2.60:

Modifications in V2.60:

The following devices have been added to the device catalog:

Changes for the gateway EU5C-SWD-PROFINET:

The format of the GSDML file has been changed from version 2.2 to version 2.25 to provide better compatibility for PROFINET configurators. The functionality used by the gateway does not change.

Back


Version notes for SWD-Assist V2.50:

Modifications in V2.50:

The following devices have been added to the device catalog:

Notes for voltage drop and current calculation:

Now the AUX voltage (24V) can be adjusted from 24V up to 28V. However, this does not change the maximum operating voltage of the connected devices. This voltage shall not be exceeded.

Changes for the gateway EU5C-SWD-EIP-MODTCP:

This gateway supports now up to 2 MBaud for SWD communication.

Back


Version notes for SWD-Assist V2.40:

Modifications in V2.40:

The following SWD gateway was added to the device catalog:

The following devices have been added to the device catalog:

Notes for voltage drop calculation at M12 cables:

The voltage drop calculation has been revised. The resistance values used at M12 lines were adapted to the cables used. This change affects only projects where M12 modules / M12 lines are used.

Cable length error with M12 cables:

If two M12 cables with different lengths were placed next to each other, the 2nd cable got the wrong length after loading the project. The order number is maintained. Now the cable length is not changed any more. Projects with this error should be corrected by deleting and reinserting the 2nd cable with the correct cable length.

Back


Version notes for SWD-Assist V2.30:

Modifications in V2.30:

The following devices have been added to the device catalog:

The following Network acessories have been added to the device catalog:

Back


Version notes for SWD-Assist V2.20:

Modifications in V2.20:

The following devices have been added to the device catalog:

The following Network acessories have been added to the device catalog:

Back


Version notes for SWD-Assist V2.10:

Modifications in V2.10:

The device catalog is now sorted by device manufacturers.

The following SWD gateway was added to the device catalog:

The following devices have been added to the device catalog:

Back


Version notes for SWD-Assist V1.92:

Modifications in 1.92:

The following devices have been added to the device catalog:

Back


Version notes for SWD-Assist V1.90:

Modifications in V1.90:

The following SWD gateway was added to the device catalog:

The following devices have been added to the device catalog:

Back


Version notes for SWD-Assist V1.80:

Modifications in V1.80:

Changed behavior of EU5C-SWD-EIP-MODTCP:

Support for firmware V1.10 has been added.

The following devices have been added to the device catalog:

Back


Version notes for SWD-Assist V1.71:

Modifications in V1.71:

Ordering options for the device EU5C-SWD-PROFINET (PROFINET SWD gateway)

For the device, a manufacturer selection has been added. The selection is made on the tab "Device parameters".

Export of the configuration for the device EU5C-SWD-PROFINET:

The exported GSDML file requires in the Gateway at least the firmware version 1.4.2.0.

The following devices have been added to the device catalog:

Back


Version notes for SWD-Assist V1.70:

Modifications in V1.70:

The following gateway was added to the device catalog:

The following SWD modules have been added to the device catalog:

Back


Version notes for SWD-Assist V1.60:

Modifications in V1.60:

The following SWD gateway was added to the device catalog:

The following SWD modules have been added to the device catalog:

The following new functions have been added to SWD-Assist:

Back


Version notes for SWD-Assist V1.50:

Modifications in V1.50:

The following SWD modules have been added to the device catalog:

Device catalog "Phoenix Contact":

An additional device catalog "Phoenix Contact" has been added.

Back


Version notes for SWD-Assist V1.41:

Modifications in V1.41:

Changed behavior of EU5C-SWD-EIP-MODTCP:

On export of the configuration as CSV file the Windows-specified separator is now used.

Changed behavior of EU5C-SWD-DP under Windows 7 64-bit:

When saving a GSD file different languages can now, as for the other operating systems, also be selected under 64-bit Windows 7.

Back


Version notes for SWD-Assist V1.40:

New functions in V1.40:

The following gateways have been added to the device catalog:

The following SWD modules have been added to the device catalog:

Communications view:

In addition to the target configuration the planned configuration can now also be compared with the SWD-Assist project or written to the SWD-Assist project.
Furthermore the SWD-Assist project can be transferred to gateway EU5C-SWD-EIP-MODTCP as set configuration.

Modified file format:

Projects that have been created with Assist V1.3x can be opened and processed with V1.40. Projects that have been stored with Assist V1.40 cannot be opened with Assist V1.3x anymore!

Back


Version notes for SWD-Assist V1.30:

New functions in V1.30:

The following devices have been added to the device catalogue:

The following universal modules are supported online:

In the Options menu, the Project Settings item has been added.
Here you can choose between "Meters, centimeters" and "Foot, inches".
The calculation of current can be toggled between "IEC/EN" and "UL/CSA" standard.
In addition, you can select whether the names in the device catalog are displayed in "Eaton US" or "Eaton EMEA" standard.

Back


Version notes for SWD-Assist V1.20:

New functions in V1.20:

The following device has been added to the device catalog:

Export of configuration for EU5C-SWD-CAN:

Through menu item "Project" →" Export configuration" the SWD configuration can be exported as module configuration for direct reuse in XSoft-CoDeSys-2.

Option "Required modules" for configurations with EU5C-SWD-CAN:

This option is shown on the "Device parameters" tab for each SWD module and can there also be disabled when creating the configuration.

Notes about device "EU5C-SWD-DP" with OS version 1.10:

Do not use the "SWD Config." button in online mode as long as the PROFIBUS-DP gateway is exchanging data with the PROFIBUS master (SWD and Config lamps on the gateway lit), as this will destroy the target configuration in the gateway. The gateway is then unable to find an SWD module on a bus restart. You can rectify this state by switching the gateway off and on again and then clicking the Config pushbutton.

Back


Version notes for SWD-Assist V1.10:

New functions in V1.10:

Device symbols:
All device have been assigned meaningful symbols.

The following devices have been added to the device catalogue:

Test and commissioning of SWD devices:

Updating operating systems:

With menu item "Help" → "Update operating systems..." you can replace the operating systems of devices EU5C-SWD-DP and EU5C-SWD-CAN.

GSD file export for Profibus DP: The GSD file is now generated language-dependent.

GSD file export for Profibus DP: The GSD file is now generated language-dependent.

Modified file format:

Projects that have been created with Assist V1.0x can be opened and processed with V1.10.
Projects that have been stored with Assist V1.10 cannot be opened with Assist V1.0x anymore!

Back


Version notes for SWD-Assist V1.01:

Modifications in V1.01:

Maximum length of the network:

The maximum length of the network has been increased from 100 m to 600 m.

Current requirement calculation:

The current consumption for the DIL-SWD-32-... interface modules has been increased by 5 mA. In individual cases this may cause the validity check to mark existing projects as invalid.

The I/O points P1 and P2 have been renamed to I0 and I1 and the description has been corrected for the interface modules DIL-SWD-32-...

The master modules EU5C-SWD-... do not have I/O points.

Back


Version notes for SWD-Assist V1.00:

Technical overview in V1.00 (first edition):

Functions for engineering and documenting an SWD configuration



Refer to the SWD-Assist Online Help for further information.